Feedback_Calibration_Current
Index.Sub | 2230.1CH |
Data Type | Unsigned16 |
Access | Read/Write |
PDO Mappable |
No |
Unit |
milliamperes (mA) |
Range |
0 to Motor max current |
Default Value | 100 |
Store Supported | Yes |
Description | This value is used for Closed Loop feature and defines motor current value used during the Feedback Calibration procedure. |
Notes |
(1) available with firmware V00r75 or superior. |