Feedback_Calibration_Speed
Index.Sub | 2230.1AH |
Data Type | Unsigned16 |
Access | Read/Write |
PDO Mappable |
No |
Unit |
0.01 rpm |
Range |
0 to 5000 |
Default Value | 500 |
Store Supported | Yes |
Description | This value is used for Closed Loop feature and defines motor speed value used during the Feedback Calibration procedure. |
Notes |
-- |