Feedback_Iq_min
| Index.Sub | 2230.0FH |
| Data Type | Unsigned16 |
| Access | Read/Write |
| PDO Mappable |
No |
| Unit |
milliamperes (mA) |
|
Range |
Unsigned16 |
| Default Value |
500 |
| Store Supported | Yes |
| Description |
This value is used for Closed Loop feature and defines minimum amplitude of the phase’s current. It can also be considered as minimum current applied at the motor. |
|
Notes |
-- |