Feedback_Kalfas
Index.Sub | 2230.0DH |
Data Type | Unsigned16 |
Access | Read/Write |
PDO Mappable |
No |
Unit |
-- |
Range |
Unsigned16 |
Default Value |
0 |
Store Supported | Yes |
Description |
This value is used for Closed Loop feature. It is used to change the advance angle depending by speed. |
Notes |
For speed value higher than 1500 rpm, set value equal to 60000. |