Feedback_Limit_Speed
| Index.Sub | 2230.1BH |
| Data Type | Unsigned16 |
| Access | Read/Write |
| PDO Mappable | RX_PDO (1) |
| Unit |
rpm |
|
Range |
0 to 4000 |
| Default Value | 3000 |
| Store Supported | Yes |
| Description | This value is used for Closed Loop feature and defines the maximum motor speed. |
|
Notes |
(1) Available with firmware V03r07 or superior. |