Feedback_Velocity_Error_Limit
| Index.Sub | 2230.1EH |
| Data Type | Unsigned32 |
| Access | Read/Write |
| PDO Mappable | No |
| Unit |
0.01 rpm |
|
Range |
Unsigned32 |
| Default Value | 1000 |
| Store Supported | Yes |
| Description | This value is used for Closed Loop feature and defines the maximum allowed displacement between motor reference velocity and motor actual velocity detected by Feedback Sensor. |
|
Notes |
-- |