Following_error_time_out
| Index.Sub | 6066.0H |
| Data Type | Unsigned16 |
| Access | Read/Write |
| PDO Mappable | No |
| Unit |
milliseconds (ms) |
|
Range |
Unsigned16 |
| Default Value | 0 |
| Store Supported | No |
| Description | When the following error occurs longer than the defined value of the time-out, the corresponding Bit13 (following error) in the Statusword will be set to one. |
|
Notes |
-- |