Home_Offset

Index.Sub 607C.0H
Data Type Integer32
Access Read/Write
PDO Mappable RX_PDO (1)
Unit User-defined position unit (2)

Range

Integer32
Default Value 0
Store Supported Yes (3)
Description  The home offset is the difference between the zero position for the application and the machine home position (found during homing). During homing the machine home position is found and once the homing is completed, the zero position is offset from the home position by adding the home offset to the home position.

Notes

(1) available with firmware V02r20 or superior.

2) See Factor Group

(3) ‘Store supported’ is available with firmware V01r36 or superior.

See Homing mode (hm).