Homing_method

Index.Sub 6098.0H
Data Type

Integer8

Access Read/Write
PDO Mappable

RX_PDO (1)

Unit --

Range

1, 2, 17, 18, 19, 20, 21, 22, 23, 24, 25, 26, 27, 28, 29, 30, 35, 37
Default Value 19
Store Supported Yes (2)
Description This object indicates the Homing method type used during the homing procedure.

Notes

(1)Available with firmware V02r20 or superior.

(2) ‘Store supported’ is available with firmware V01r36 or superior.

See Homing mode (hm).