Max_Torque

Index.Sub 6072.0H
Data Type Unsigned16
Access Read/Write
PDO Mappable RX_PDO (1)
Unit ‰ Nominal_Current

Range

0 to (‰ Max drive current)
Default Value 1000
Store Supported Yes
Description

This object defines the maximum torque for Profile Torque mode (tq) (tq) and Cyclic Synchronous Torque (cst) modes. The value is considered proportional to Nominal_Current (Motor rated current).

The value is defined as thousandths of the torque, e.g. ‘500’ means ‘50%’ of the Motor rated torque. 

Notes

(1) available with firmware V03r03 or superior.

This object is available only with firmware version V03r03 or superior.