Min_Current
| Index.Sub | 2005.1H |
| Data Type | Unsigned16 |
| Access | Read/Write |
| PDO Mappable | RX_PDO (1) |
| Unit |
milliamperes (mA) |
|
Range |
0 to Max drive current |
| Default Value | 0 |
| Store Supported | Yes |
| Description |
It sets the motor’s reduced current. The drive automatically reduces the current after a current reduction time at the end of the movement. This object is used for Open Loop. |
|
Notes |
|