Preset_Homing_Position

Index.Sub

2080.0H

Data Type Integer32
Access Read/Write
PDO Mappable No
Unit User-defined position unit (1)

Range

Integer32
Default Value 0
Store Supported Yes
Description

This object is used during the Homing mode procedure and contains the desired position value for the Homing Zero Position. All position values for the following objects are set to  Preset_Homing_Position value: Position_demand_value (6062.0H), Position_Actual_Internal_Value (6063.0H), Position_Actual_Value (6064.0H) are set to  Preset_Homing_Position value.

Notes

(1) See Factor Group.

(2) ‘Store supported’ is available with firmware V01r36 or superior.