Quick_stop_option_code
| Index.Sub | |
| Data Type |
Integer16 |
| Access | Read/Write |
| PDO Mappable | No |
| Unit | -- |
|
Range |
0 = Disable drive function, motor is free to rotate 2 = Slow down with quick stop ramp and transit into Switch On Disabled 6 = Slow down with quick stop ramp and stay in Quick Stop Active |
| Default Value | 0 |
| Store Supported | Yes (1) |
| Description | This parameter determines what action should be taken if the Quick Stop Function is executed. |
|
Notes |
(1) ‘Store supported’ is available with firmware V01r38 or superior. |