Torque_demand

Index.Sub 6074.0H
Data Type

Integer16

Access Read Only
PDO Mappable TX_PDO (1)
Unit ‰ Nominal_Current

Range

0 to (‰ Max drive current)
Default Value 0
Store Supported No
Description

This object is used for Profile Torque mode (tq) and Cyclic Synchronous Torque (cst) modes and provides the actual torque value of the trajectory generator. The value is considered proportional to Nominal_Current (Motor rated current). The value is defined as thousandths of the torque, e.g. ‘500’ means ‘50%’ of the Motor rated torque.  

Notes

(1) available with firmware V03r03 or superior.

  • This object is available only with firmware version V03r03 or superior.