Velocity_Actual_Value
| Index.Sub | 606C.0H |
| Data Type | Integer32 |
| Access | Read Only |
| PDO Mappable | TX_PDO (1) |
| Unit | User-defined velocity unit (2) |
|
Range |
Integer32 |
| Default Value | 0 |
| Store Supported | No |
| Description | This object contains the current velocity of the motor. |
|
Notes |
(1)Available with firmware V00r74 or superior. (2)See Factor Group. |