COGCOMP.CORRECTIONTABLE

Description

Reads or writes to the cogging compensation table.

Examples

Reads the full table:

COGCOMP.CORRECTIONTABLE

Reads the compensation value for index "x":

COGCOMP.CORRECTIONTABLE x

Writes the value "y" to the table at index "x":

COGCOMP.CORRECTIONTABLE x y

General Information

Type

R/W Parameter

Units

mA

Range

Argument 1: 0 to 8,191

Argument 2: 1.628 * DRV.IPEAK

Default Value

0

Data Type

Integer

Start Version

M_01-14-06-001

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC No
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.