DRV.IPEAK

Description

DRV.IPEAK returns the drive peak rated current in Arms.

General Information

Type

R/O Parameter

Units

Arms

Range

N/A

Default Value

N/A

Data Type

Float

Start Version

M_01-00-00-000
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
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

5084h /0

M_01-00-00-000

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2132 DWord Yes
Sercos® III 4 Octets
EtherNet/IP
Instance Data Size Data Type
133 4 Byte Signed Float
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

264

No 32 bit Yes M_01-03-00-000

Related Topics

"Foldback"

DRV.ICONT