DOUT.STATES

Description

DOUT.STATES reads the states of the digital output. The leftmost bit represents DOUT1 and the rightmost bit represents DOUT2.


  • AKD-C only reads the state of DOUT1.

General Information

Type

R/O Parameter

Units

N/A

Range

0 to 11

Default Value

N/A

Data Type

String

BASIC: Integer

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKDCANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherNet/IP
Instance Data Size Data Type
98 N/A Integer Array
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

194

No 8 bit No M_01-03-00-000

Related Topics

Digital Outputs