DRV.CUSTOMIDENTIFIER
Description
Use DRV.CUSTOMIDENTIFIER to assign a unique string to a device. The string must use the following formatting rules:
- ASCII characters only
- 32 character max length
- No spaces in string
The string is displayed on the device overview screen and in the start page's device discovery table.
General Information
Type |
NV Parameter |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
String |
Start Version |
M_01-12-05-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet | Yes* |
AKD EtherNet/IP | Yes |
AKD Profinet | Yes |
AKD sercos® III | Yes |
AKD-N | Yes |
AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus | Index/Subindex | Object Start Version |
---|---|---|
EtherCAT COE and CANopen |
2032h/0 |
M_01-12-05-000 |
Related Topics