DRV.MOTIONDISSOURCES
Description
This parameter reports some of the reasons that motion may not be allowed on the axis. There are additional reasons why the drive cannot accept a motion command that are not reported by this command (for example, fieldbus control bits or fault status).
Value | Description |
---|---|
0 | Motion not blocked by reason indicated for value 1, 2, or 3. |
1 | Suspend Motion Active |
2 | Brake not released |
4 | Brake not released |
8 | Rotor flux not ready |
General Information
Type |
R/O Parameter |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
Integer |
Start Version |
M_01-10-03-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet | Yes* |
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus |
Address |
Attributes | Signed? |
---|---|---|---|
Profinet |
2891 |
Word | No |
sercos® III | 2 Octets |
Fieldbus | Instance | Data Size | Data Type |
---|---|---|---|
EtherNet/IP | 892 | 2 Byte | Integer |
Related Topics