HOME.MODE
Description
HOME.MODE specifies the homing procedure of the drive. The homing modes available in the drive are summarized in the following table; see Homing for a detailed discussion and examples for each mode:
Mode | Description |
---|---|
0 |
Home using current position |
1 |
Find limit input |
2 |
Find input limit then find zero angle |
3 |
Find input limit then find index |
4 |
Find home input, including hardware limit switches |
5 |
Find home input then find zero angle, including hardware limit switches |
6 |
Find home input then find index, including hardware limit switches. |
7 |
Find zero angle |
8 |
Move until position error exceeded |
9 |
Move until position error exceeded, then find zero angle |
10 |
Move until position error exceeded, then find index |
11 |
Find index signal, without any precondition |
12 |
Homing to a home-switch, including mechanical stop detection |
13 | Home using the feedback position |
14 | Homing to a home-switch for rotary applications |
15 | Find next feedback zero position |
16 | Find home input with dual edges |
17 | Absolute Mode - Calculate and save offset |
18 | Find home input, then find next feedback zero position |
General Information
Type |
R/W Parameter |
Units |
N/A |
Range |
0 to 18 |
Default Value |
0 |
Data Type |
Integer |
See Also |
N/A |
Start Version |
M_01-00-00-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet | Yes* |
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus |
Index/Subindex |
Object Start Version |
---|---|---|
EtherCAT COE and CANopen |
M_01-00-00-000 |
Fieldbus |
Address |
Attributes | Signed? |
---|---|---|---|
Profinet |
2203 |
Word | No |
sercos® III | 2 Octets |
Fieldbus | Instance | Data Size | Data Type |
---|---|---|---|
EtherNet/IP | 204 | 2 Byte | Integer |
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? | Object Start Version |
---|---|---|---|---|---|
Modbus |
406 |
No | 16 bit | No | M_01-03-00-000 |
Related Topics