IL.DIFOLD

Description

IL.DIFOLD is the output of the drive foldback algorithm. It is an artificial current, which can be higher or lower than the drive peak current (DRV.IPEAK). When IL.DIFOLD is lower than the existing current limit (such as IL.LIMITP), it becomes the active current limit.

IL.DIFOLD decreases when the actual current is higher than drive continuous current and increases (up to a certain level) when the actual current is lower than drive continuous current.

General Information

Type

R/O Parameter

Units

Arms

Range

0 to 2,147,483.647 Arms

Default Value

N/A

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen ]
Index/Subindex Object Start Version
3559h/0 M_01-00-00-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2833 DWord No
Sercos® III 4 Octets
EtherNet/IP
Instance Data Size Data Type
834 4 Byte Float
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version
1666 No 32-bits No M_01-06-03-000

Related Topics

"Current Loop"