IL.FBSOURCE

Description

This parameter selects the feedback source that current loop uses for commutation angle calculation. It applies only when MOTOR.TYPE = 4.

0 = Primary feedback

1 = Secondary feedback

2 = Tertiary feedback

When IL.FBSOURCE is changed, MOTOR.POLES and MOTOR.PHASE are updated.

IL.FBSOURCE MOTOR.PHASE is set to: MOTOR.POLES is set to:
0 FB1.MOTORPHASE FB1.MOTORPOLES
1 FB2.MOTORPHASE FB2.MOTORPOLES
2 FB3.MOTORPHASE FB3.MOTORPOLES

For induction motor closed loop control the commutation angle is set as shown in the following figure.

General Information

Type

R/W

Units

N/A

Range

0 to 2

Default Value

0

Data Type

Integer

Start Version

M_01-08-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N No
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

5361h /0

M_01-08-00-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2865 Byte No
Sercos® III 2 Octets
EtherNet/IP
Instance Data Size Data Type
866 1 Byte Integer
Modbus
Register Address Is 64 bit? Attributes Signed?
1730 No 8-bit No

Related Topics

MOTOR.TYPE

FB1.MOTORPOLES | FB2.MOTORPOLES | FB3.MOTORPOLES

FB1.MOTORPHASE | FB2.MOTORPHASE | FB3.MOTORPHASE