IL.MFOLDR

Description

IL.MFOLDR sets the recovery time for the motor foldback algorithm. If 0 current is applied for at least the recovery time duration, it is possible to apply motor peak current for the duration of IL.MFOLDD time.

The IL.MFOLDR value is automatically calculated from other foldback parameters.

General Information

Type

R/O Parameter

Units

s

Range

0.1 to 65,535 s

Default Value

Calculated from other foldback parameters.

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2233 DWord No
Sercos® III 4 Octets
EtherNet/IP
Instance Data Size Data Type
234 4 Byte Float
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

466

No 32 bit No M_01-03-00-000

Related Topics

Current Loop