IL.VCMD

Description

Reads the output of the current loop that controls the q-component of the current.

General Information

Type

R/O Parameter

Units

Vrms

Range

0 Vrms to bus voltage

Default Value

N/A

Data Type

Integer

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2237 Word Yes
Sercos® III 2 Octets
EtherNet/IP
Instance Data Size Data Type
238 2 Byte Signed Float
Modbus
Register Adddress Is 64 bit? Attributes Signed? Object Start Version

474

No 16 bit Yes M_01-03-00-000

Related Topics

Current Loop