IL.VVFB

Description

The range for this parameter depends on whether the drive model is an MV/240 VAC or an HV/480 VAC. 

The VBusScale parameter sets the drive model:

MV/240 VAC:  VBusScale = 1

HV/480 VAC:  VBusScale = 2

VBusScale is used for multiple parameter ranges that are model dependent, such as IL.KP.

General Information

Type

R/O Parameter

Units

V

Range

–1200*VBusScale to +1200*VBusScale

Default Value

N/A

Data Type

Integer

See Also

IL.VUFB

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2239 Word Yes
Sercos® III 2 Octets
EtherNet/IP
Instance Data Size Data Type
240 2 Byte Signed Integer
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

478

No 16 bit Yes M_01-03-00-000

Related Topics

Current Loop