MOTOR.TEMPC

Description

When the motor has a thermistor with linear characteristics (MOTOR.RTYPE = 2, 3 or 4), MOTOR.TEMPC returns the motor temperature in degrees Celsius, which is calculated from the resistance of the motor thermistor.

There is no algorithm to convert from resistance to degrees Celsius for non-linear thermistors. In this case, MOTOR.TEMPC returns -32,768 which is an invalid temperature.

General Information

Type

R/O Parameter

Units

Degrees Celsius

Range

-215 to 215

Default Value

N/A

Data Type

Integer

Start Version

M_01-10-04-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3458h/0 M_01-10-04-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2900 Word No
Sercos® III 2 Octets
EtherNet/IP
Instance Data Size Data Type
901 2 Byte Integer
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

1800

No 16 bit No M_01-03-00-000

Related Topics

"Motor View" | MOTOR.TEMP | MOTOR.RTYPE