REC.TRIGTYPE

Description

REC.TRIGTYPE sets the type of trigger.

Input values are as follows:

Value Description

0

Recording starts immediately

1

Recording starts on the next command executed through the TCP/IP. The trigger location in the buffer is set according to REC.TRIGPOS.

2

Recording starts per the values of REC.TRIGPARAM, REC.TRIGVAL, REC.TRIGSLOPE, and REC.TRIGPOS.

3

Recording starts when the value of REC.TRIGPARAM is 0 for REC.TRIGSLOPE = 0 or 1 for REC.TRIGSLOPE = 1

General Information

Type

R/W Parameter

Units

0 = immediate

1 = command

2 = parameter

3 = boolean

Range

0 to 3

Default Value

0

Data Type

Integer

See Also

REC.TRIG, REC.TRIGPARAM, REC.TRIGVAL, REC.TRIGSLOPE REC.TRIGPOS

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III

Fieldbus

Address

Attributes Signed?

PROFINET

2364 Byte No
Sercos® III 2 Octets
EtherNet/IP
Instance Data Size Data Type
365 1 Byte Integer
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

728

No 8 bit No M_01-03-00-000

Related Topics

Scope