REC.TRIGVAL

Description

REC.TRIGVAL is the value that must be met by REC.TRIGPARAM for the trigger to occur. The units of this parameter are set according to the units of REC.TRIGPARAM.

General Information

Type

R/W Parameter

Units

The units of the parameter are chosen according to the unit type.

Range

-9223372036854775.808 to 9223372036854775.807

Default Value

0

Data Type

Integer

See Also

REC.TRIG, REC.TRIGPARAM, REC.TRIGVAL, REC.TRIGSLOPE, REC.TRIGPOS

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2365 DWord Yes
Sercos® III 8 Octets
EtherNet/IP
Instance Data Size Data Type
366 8 Byte Signed Varies
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

730

Yes 64 bit Yes M_01-03-00-000

Related Topics

Scope