REGEN.TESTVTHRESH

REGEN.TESTVTHRESH sets the voltage threshold for the REGEN.TEST command.

General Information

Type Command
Description Sets regen test voltage threshold.
Units %
Range 1 – 99 %
Default Value 80 %
Data Type Integer
Start Version M_01-18-06-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKDEtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N No
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Related Topics

Regeneration