VDIN.STATES

Description

VDIN.STATES reads the states of the virtual digital inputs. Bit 0 represents virtual digital input 1 (VDIN1) and bit 7 represents virtual digital input 8 (VDIN8).

General Information

Type

 R/O Parameter

Units

N/A

Range

00h to FFh

Default Value

N/A

Data Type

Integer

See Also

N/A

Start Version

M_01-22-01-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT COE and CANopen
Index/Subindex Object Start Version

3476h/1

VDIN.STATES M_01-22-01-000
PROFINET and Sercos® III
Command Fieldbus Address Attributes Signed?
VDIN.STATES

PROFINET

3192 Byte No
Sercos® III 2 Octets
EtherNet/IP
Parameter Instance Data Size Data Type
VDIN.STATES 1193 1 Byte   Integer
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version
3200 VDIN.STATES No 16 bit No M_01-22-01-000

Related Topics

Digital Inputs and Outputs