VDIN1.INV to VDIN8.INV

Description

Sets the indicated polarity of a virtual digital input mode.

Context

For more information on EtherCAT CoE/CANopen, see subindex 3 under Object 3476: Virtual digital inputs settings.

Example

VDIN1.INV = 0: Virtual input is active high.

VDIN1.INV = 1: Virtual input is active low.

General Information

Type

 R/W Parameter

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Boolean

See Also

N/A

Start Version

M_01-22-01-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Parameter Fieldbus Address Attributes Signed?
VDIN1.INV

PROFINET

3176 Byte No
Sercos® III 2 Octets
VDIN2.INV

PROFINET

3177 Byte
Sercos® III 2 Octets
VDIN3.INV

PROFINET

3178 Byte
Sercos® III 2 Octets
VDIN4.INV

PROFINET

3179 Byte
Sercos® III 2 Octets
VDIN5.INV

PROFINET

3180 Byte
Sercos® III 2 Octets
VDIN6.INV

PROFINET

3181 Byte
Sercos® III 2 Octets
VDIN7.INV

PROFINET

3182 Byte
Sercos® III 2 Octets
VDIN8.INV

PROFINET

3183 Byte
Sercos® III 2 Octets
EtherNet/IP
Parameter Instance Data Size Data Type
VDIN1.INV 1177 1 Byte   Integer
VDIN2.INV 1178
VDIN3.INV 1179
VDIN4.INV 1180
VDIN5.INV 1181
VDIN6.INV 1182
VDIN7.INV 1183
VDIN8.INV 1184
Modbus
Parameter Register Address Is 64 bit? Attributes Signed? Object Start Version
VDIN1.INV

3168

No 8 bit No M_01-22-01-000
VDIN2.INV 3170
VDIN3.INV 3072
VDIN4.INV 3174
VDIN5.INV 3176
VDIN6.INV 3178
VDIN7.INV 3180
VDIN8.INV 3180

Related Topics

Digital Inputs and Outputs