VL.ARPF1 TO VL.ARPF4

Description

VL.ARPF1 sets the natural frequency of the pole (denominator) of AR filter 1. This value is FP in the approximate transfer function of the filter:

ARx(s) = [s²/(2πFZ)² +s/(QZ2πFZ) + 1]/ [s²/(2πFP)² +s/(QP2πFP) + 1]

 

The following block diagram describes the AR filter function; note that AR1 and AR2 are in the forward path, while AR3 and AR4 are applied to feedback:

AR1, AR2, AR3, and AR4 are used in velocity and position mode, but are disabled in torque mode.

Discrete time transfer function (applies to all AR filters)

The velocity loop compensation is actually implemented as a digital discrete time system function on the DSP. The continuous time transfer function is converted to the discrete time domain by a backward Euler mapping:

s ≈ (1-z-1)/t, where t = 62.5 µs

The poles are prewarped to FP and the zeros are prewarped to FZ.

General Information

Type

R/W Parameter

Units

Hz

Range

5 to 5,000 Hz

Default Value

VL.ARPF1: 675 Hz

VLARPF2 to VLARPF4: 500 Hz

Data Type

Float

See Also

VL.ARPQ1 TO VL.ARPQ4, VL.ARZF1 TO VL.ARZF4, VL.ARZQ1 TO VL.ARZQ4

Start Version

M_01-02-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3406h/1

VL.ARPF1

M_01-02-00-000

3406h/2

VL.ARPF2

3406h/3

VL.ARPF3

3406h/4

VL.ARPF4

PROFINET and Sercos® III
Parameter Fieldbus Address Attributes Signed?
VL.ARPF1 PROFINET

2404

DWord No
Sercos® III 4 Octets
VL.ARPF2 PROFINET 2405 DWord
Sercos® III 4 Octets
VL.ARPF3 PROFINET 2406 DWord
Sercos® III 4 Octets
VL.ARPF4 PROFINET 2407 DWord
Sercos® III 4 Octets
EtherNet/IP
Parameter Instance Data Size Data Type
VL.ARPF1 405 4 Byte Float
VL.ARPF2 406
VL.ARPF3 407
VL.ARPF4 408
Modbus
Parameter  Register Address Is 64 bit? Attributes Signed? Object Start Version
VL.ARPF1 808 No 32 bit No M_01-03-00-000
VL.ARPF2 810
VL.ARPF3 812
VL.ARPF4 814

Related Topics

"Velocity Loop"