VL.ARPQ1 TO VL.ARPQ4

Description

VL.ARPQ1 sets the Q (quality factor) of the pole (denominator) of AR filter 1. This value is QP in the approximate transfer function of the filter:

 

ARx(s) = [s²/(2πFZ)²+s/(QZ2πFZ) + 1]/ [s²/(2πFP)² +s/(QP2πFP) + 1]

 

The following block diagram describes the AR filter function; note that AR1 and AR2 are in the forward path, while AR3 and AR4 are applied to feedback:

AR1, AR2, AR3, and AR4 are used in velocity and position mode, but are disabled in torque mode.

Discrete time transfer function (applies to all AR filters)

The velocity loop compensation is actually implemented as a digital discrete time system function on the DSP. The continuous time transfer function is converted to the discrete time domain by a backward Euler mapping:

s ≈ (1-z-1)/t, where t = 62.5 µs

The poles are prewarped to FP and the zeros are prewarped to FZ.

General Information

Type

R/W Parameter

Units

None

Range

0.2 to 20

Default Value

VL.ARPQ1: 0.707

VLARPQ2 to VLARPQ4: 0.5

Data Type

Float

See Also

VL.ARPF1 TO VL.ARPF4, VL.ARZF1 TO VL.ARZF4, VL.ARZQ1 TO VL.ARZQ4

Start Version

M_01-02-00-000
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3406h/5

VL.ARPQ1

M_01-02-00-000

3406h/6

VL.ARPQ2

3406h/7

VL.ARPQ3

3406h/8

VL.ARPQ4

PROFINET and Sercos® III
Parameter Fieldbus Address Attributes Signed?
VL.ARPQ1 PROFINET

2408

DWord No
Sercos® 4 Octets
VL.ARPQ2 PROFINET 2409 DWord
Sercos® III 4 Octets
VL.ARPQ3 PROFINET 2410 DWord
Sercos® III 4 Octets
VL.ARPQ4 PROFINET 2411 DWord
Sercos® III 4 Octets
EtherNet/IP
Parameter Instance Data Size Data Type
VL.ARPQ1 409 4 Byte Float
VL.ARPQ2 410
VL.ARPQ3 411
VL.ARPQ4 412
Modbus
Parameter  Register Address Is 64 bit? Attributes Signed? Object Start Version
VL.ARPQ1 816 No 32 bit No M_01-03-00-000
VL.ARPQ2 818
VL.ARPQ3 820
VL.ARPQ4 822

Related Topics

"Velocity Loop"