VL.MODEL

Description

VL.MODEL is the observer velocity output. When VL.KO is tuned properly, VL.MODEL will match VL.FB, except when there is an unspecified offset between the two.

General Information

Type

R/O Parameter

Units

Depends on UNIT.VROTARY or UNIT.VLINEAR, UNIT.ACCLINEAR

Rotary: rpm, rps, deg/s, (custom units)/s, rad/s

Linear: counts/s, mm/s, μm/s, (custom units)/s

Range

N/A

Default Value

N/A

Data Type

Float

See Also

VL.FB, VL.KO

Start Version

M_01-00-01-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Fieldbus Parameter Address Attributes Signed?

PROFINET

VL.MODEL_32 2441 DWord Yes
Sercos® III 8 Octets
EtherNet/IP
Instance Data Size Data Type
442 8 Byte Signed Velocity
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

882

Yes low 32 bit word Yes M_01-03-00-000

Related Topics

Velocity Loop