WS.CHECKT

Description

This parameter sets the amount of time a commutation error must be present before an error is thrown. Commutation monitoring is disabled when this parameter is set to 0.

General Information

Type

R/W Parameter

Units

ms

Range

0 to 10,000

Default Value

N/A

Data Type

U16

Start Version

M_01-06-03-000
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

5352h /0

M_01-06-03-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2850 Word No
Sercos® III 2 Octets
EtherNet/IP
Instance Data Size Data Type
851 2 Byte Integer
Modbus

Register Address

Is 64 bit? Attributes Signed? Object Start Version

1700

No 16-bit No

M_01-06-03-000

Related Topics

Wake and Shake Overview | WS.CHECKV