AXIS#.EIP.STREAMPERIOD

Description

This parameter allows modifying and configuring the interval at which the drive expects to receive position set-points from the fieldbus master when position streaming is configured and enabled (AXIS#.EIP.STREAMING = 1).

Example

-->AXIS1.EIP.STREAMPERIOD 500
-->AXIS1.EIP.STREAMPERIOD
500 [us]

Versions

Action Version Notes
Implemented 02-11-00-001

General Information

Type

Read/Write

Units

Microseconds

Range

500 to 10000

Default Value

2000

Data Type

AXIS#.EIP.STREAMING

Stored in Non-Volatile Memory

Yes

Variants Supported

EtherNet/IP drives: AKD2G-SPI

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.EIP.QUICKSTOPACTION

7554

1D82

Signed16

Read/Write

-

AXIS2.EIP.QUICKSTOPACTION

73090

11D8

Signed16

Read/Write

-