AXIS#.GEAR.AUTOSTART

Description

The command AXIS#.GEAR.AUTOSTART determines whether or not gearing begins when the axis is enabled or transitions into Command Source: Electronic Gearing.

If AUTOSTART is enabled then electronic gearing immediately begins and tries to achieve synchronization with the master.

If AUTOSTART is disabled, issue AXIS#.GEAR.MOVE before synchronization begins.

Versions

Action Version Notes
Implemented 02-07-00-000

General Information

Type

Parameter

Description

Determines whether gearing autostarts or requires manual start.

Units

N/A

Range

0 (Disabled) – 1 (Enabled)

Default Value

1 (Enabled)

Data Type

Integer

See Also

N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Related Topics

Electronic Gearing