AXISx.IL.IUCMD

Description

AXIS#.IL.IUCMD reports the actual phase U current command after limits have been applied to AXISx.IL.IUCMDU. It is in use when AXIS#.OPMODE = 0 (Torque mode) and AXISx.IL.CMDMODE = 1 (Phase Current mode).

Versions

Action Version Notes
Implemented 02-07-03-000

General Information

Type Read only
Units Arms
Range Same as AXISx.IL.IUCMDU range
Default Value N/A
Data Type Float
See Also AXISx.IL.CMDMODE, AXISx.IL.IUCMDU, AXISx.IL.SETCMD
Stored in Non-Volatile Memory N/A

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.IUCMD

5834

16CA

Signed32

Read Only

-

AXIS2.IL.IUCMD

71370

116C

Signed32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.IUCMD

5834

Float

Read Only

-

Related Topics

Current Loop