AXIS#.OPMODE
Description
AXIS#.OPMODE specifies the operation mode of the axis. AXIS#.CMDSOURCE must also be used to set the source of the command to the axis.
The operation mode values can be set as follows:
Mode |
Description |
---|---|
0 |
Current (torque) operation mode |
1 |
Velocity operation mode |
2 |
Position operation mode |
AXIS#.OPMODE can be changed while the axis is enabled or disabled. If using the terminal to change the operation mode, it is recommended to disable the axis before changing the operation mode. If changing the operation mode from the terminal while the axis is enabled, the system may experience a step change in demand.
Example
Set the source of the command to a TCP/IP channel and the desired operation mode to velocity:
-->AXIS1.CMDSOURCE 0
-->AXIS1.OPMODE 1
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 2 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Gantry Mode
If the axis is in Gantry Mode (CMDSOURCE = 4), then this opmode setting has no effect until the CMDSOURCE is set to something other than 4 – Gantry.
Sensorless Field Oriented Control Mode
If sensorless field oriented control is activated by setting AXIS#.IL.FBSOURCE=100, only velocity mode can be selected as the opmode.
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT COE and CANopen | AXIS1.OPMODE | 0x5000 | 0x5 | USINT | - | - | RW | False |
AXIS2.OPMODE | 0x5100 | 0x5 | USINT | - | - | RW | False |