AXISx.IL.IVCMD
Description
AXIS#.IL.IVCMD reports the actual phase V current command after limits have been applied to AXISx.IL.IVCMDU. It is in use when AXIS#.OPMODE = 0 (Torque mode) and AXISx.IL.CMDMODE = 1 (Phase Current mode).
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-07-03-000 |
General Information
Type | Read only |
Units | Arms |
Range | Same as AXISx.IL.IVCMDU range |
Default Value | N/A |
Data Type | Float |
See Also | AXISx.IL.CMDMODE, AXISx.IL.IVCMDU, AXISx.IL.SETCMD |
Stored in Non-Volatile Memory | N/A |
Variants Supported
All variants are supported.
Fieldbus Information
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.IL.IVCMD |
5835 |
16CB |
Signed32 |
Read Only |
- |
AXIS2.IL.IVCMD |
71371 |
116C |
Signed32 |
Read Only |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.IL.IVCMD |
5835 |
Float |
Read Only |
- |