AXIS#.PL.CMD.MWOFFSET

Description

Position MechaWare (MW) offset is a MW block which adds position to Position command and is designed to interact with MW user models.

Versions

Action Version Notes
Implemented 02-05-05-000

 

Revised 02-08-02-000 Renamed from AXISx.PL.MWFF

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units.

Range

Depends on units. See Position Range.

Default Value

0

Data Type

Float

See Also AXIS#.IL.MWFF, AXIS#.VL.MWFF

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.PL.CMD.MWOFFSET

5921

1721

Signed32

Read/Write

Position

AXIS2.PL.CMD.MWOFFSET

71457

1172

Signed32

Read/Write

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.CMD.MWOFFSET

5921

Signed32

Read/Write

Position