AXIS#.VL.MWFF

Description

Velocity MechaWare (MW) feed forward is a MW block which adds velocity to velocity command and designed to interact with MW user models.

Versions

Action Version Notes
Implemented 02-05-05-000

 

General Information

Type

Read/Write

Units

Depends on AXIS#.UNIT.VROTARY

Rotary: rpm, rps, deg/s, custom units/s, rad/s

Range

Rotary

-15,000.000 to 15,000.000 rpm

-250.000 to 250.000 rps

-90000.000 to 90000.000 deg/s

-1250.000 to 1250.000 custom units/s

-1570.796 to 1570.796 rad/s.

Default Value

0

Data Type

Float

See Also AXIS#.IL.MWFF, AXIS#.PL.CMD.OFFSET

Stored in Non-Volatile Memory

No