AXIS#.PL.KFB.POUT
Please refer to AXIS#.PL.KFB.PIN for details.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-08-01-000 |
General Information
Type | Read/Write |
Units | N/A |
Range | 1 to 2,147,483,647 |
Default Value | 1 |
Data Type | Integer |
See Also | AXIS#.PL.KFB, AXIS#.PL.KFB.PIN, AXIS#.VL.KFB |
Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.PL.KFB.POUT |
500ch |
12h |
Signed32 |
- |
- |
Read/Write |
No |
AXIS2.PL.KFB.POUT |
510ch |
12h |
Signed32 |
- |
- |
Read/Write |
No |