AXIS#.PL.KFB
Refer to AXIS#.PL.KFB.PIN for details.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-08-00-000 |
General Information
Type | Read/Write |
Units | N/A |
Range | - 2,147,483,648 to 2,147,483,647 |
Default Value | 1.0 |
Data Type | Float |
See Also | AXIS#.PL.KFB.PIN, AXIS#.PL.KFB.POUT |
Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT COE and CANopen | AXIS1.PL.KFB | 0x500C | 0x0D | UINT | 1:1 | - | W | False |
AXIS2.PL.KFB | 0x510C | 0x0D | UINT | 1:1 | - | W | False |