AXIS#.VL.LIMITN
Description
AXIS#.VL.LIMITN sets the velocity command negative limit.
If the input to the velocity loop is lower than AXIS#.VL.LIMITN, then the actual velocity command AXIS#.VL.CMD is limited by the value of AXIS#.VL.LIMITN.
-
-
ECCN 3A255 imposes special limitations on operating speed for induction motors. See ECCN 3A225 Limitations for Induction Motors.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s See Velocity Units for details. |
Range |
Depends on units. See Velocity Range for details. |
Default Value |
15000 RPM Depends on units. See Velocity Units for details. |
Data Type |
Float |
See Also |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT COE and CANopen | AXIS1.VL.LIMITN | 0x5011 | 0x7 | DINT | - | Velocity | RW | False |
AXIS2.VL.LIMITN | 0x5111 | 0x7 | DINT | - | Velocity | RW | False |