EIP.SYNCINFO

Description

EIP.SYNCINFO provides detailed information about the drive’s time sync object, which is required by the CIP Sync connection. This information aids in troubleshooting potential timing issues between the drive and controller.

Versions

Action Version Notes
Implemented 02-10-00-000

General Information

Variants Supported

EtherNet/IP drives: AKD2G-SPI

See Also

EIP.PLLMODE | CIP Sync Command Assembly Data Structure (105) | CIP Sync Response Assembly Data Structure (106)