FB#.ENCLINES

Description

Used to configure the number of lines per revolution for rotary encoders. This keyword is only valid for Incremental and Sin/Cos encoders and is ignored for any other encoders and linear motors.

Context

See Feedback Settings.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Lines/revolution

Range

0 to 4,294,967,288

Default Value

1024

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCAT COE and CANopen FB1.ENCLINES 0x3500 0x2 UDINT - - RW False
FB2.ENCLINES 0x3501 0x2 UDINT - - RW False
FB3.ENCLINES 0x3502 0x2 UDINT - - RW False
FB4.ENCLINES 0x3503 0x2 UDINT - - RW False
FB5.ENCLINES 0x3504 0x2 UDINT - - RW False