FB#.MULTITURNBITS

Description

Number of multi-turn bits used for BiSS encoders when used in rotary motors. This is specified by the feedback datasheet.

Context

Only used when FB#.MECHTYPE is rotary and identified feedback is BiSS. See Feedback Settings.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

multi-turn bits

Range

0 to 32

Default Value

12

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.