FB#.RESKTR

Description

This parameter sets the resolver nominal transformation ratio. It affects the resolver excitation output amplitude.

The value is obtained from the resolver data sheet.

Context

See Feedback Settings.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0.001 to 50.000

Default Value

0.5

Data Type

Float

See Also

N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCAT COE and CANopen FB1.RESKTR 0x3500 0x4 UDINT - - RW False
FB2.RESKTR 0x3501 0x4 UDINT - - RW False
FB3.RESKTR 0x3502 0x4 UDINT - - RW False
FB4.RESKTR 0x3503 0x4 UDINT - - RW False
FB5.RESKTR 0x3504 0x4 UDINT - - RW False